AXIS#​.FIELDWEAKENING​.VBUSMARGIN

Description

AXIS#.FIELDWEAKENING.VBUSMARGIN determines the field-weakening-loop’s threshold voltage with respect to the bus voltage in [%]. By default, this value is set to 95%, meaning if the magnitude of the motor-voltage vector tries to go above 95% of bus voltage, the field weakening algorithm activates. Once activated, it maintains the motor-voltage vector magnitude at 95% of bus voltage. It applies whatever d-axis current necessary to reduce the induced back-emf-voltage of the motor to create the commanded q-axis current.

  • Setting this value to higher than 95% means having less voltage margin for the voltage regulation but results in higher voltage utilization.
  • Setting this value to lower than 95% means having higher voltage margin for the voltage regulation but results in lower voltage utilization.

Versions

Action Version Notes
Implemented 02-06-00-000

 

General Information

Type

Read/Write

Units

%

Range

0 to 100%

Default Value

95

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.FIELDWEAKENING.VBUSMARGIN

5019h

03h

Signed32

-

-

Read/Write

No

AXIS2.FIELDWEAKENING.VBUSMARGIN

5119h

03h

Signed32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.FIELDWEAKENING.VBUSMARGIN

7303

1C87

Signed32

Read/Write

-

AXIS2.FIELDWEAKENING.VBUSMARGIN

72839

11C8

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FIELDWEAKENING.VBUSMARGIN

7303

Signed32

Read/Write

-